This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TINA/Spice: ECH8654/ECH8667 spice models

Other Parts Discussed in Thread: TINA-TI

Tool/software: TINA-TI or Spice Models

Hi everyone,

how I can import models for ECH8654/ECH8667 MOSFET in TINA.-TI?

There isn't SUBCKT directive, but only MODEL one.

Thank you.

Regards,

Michele

********************** ECH8654 SPICE PARAMETER *************************
.LIB ECH8654                                                                  
* DATE : 2007/10/29                                                           
* Temp = 27 deg                                                               
* W    =  1494310 E-6 m                                                       
* L    =      1.0 E-6 m                                                       
* AD   =  1494310 E-12 m2                                                     
* RG   =       15 ohm                                                         
* RB   =    0.013 ohm                                                         
                                                                              
.MODEL ECH8654 PMOS (                                LEVEL    = 8             
+VERSION  = 3.2            TNOM     = 27             TOX      = 2.7E-08       
+VTH0     = -0.91          K1       = 1.96           K2       = -0.04         
+NLX      = 3.20E-07       DVT0     = 1.12           DVT1     = 0.22          
+DVT2     = -0.01          U0       = 300            UA       = 1.10E-10      
+UB       = 1.00E-21       VSAT     = 1.86E04        A0       = 0.44          
+AGS      = 1.00           A1       = 0              A2       = 1             
+RDSW     = 2.96E03        PRWG     = -0.011         WR       = 0.83          
+WINT     = 0              LINT     = 2.09E-09       VOFF     = -0.10         
+NFACTOR  = 1.118          CIT      = 0              CDSC     = 2.40E-04      
+CDSCD    = 0              ETA0     = 0.08           DSUB     = 0.96          
+PCLM     = 1.40           PDIBLC1  = 0.05           PDIBLC2  = 6.50E-03      
+DROUT    = 0.96           PSCBE1   = 1.40E09        PSCBE2   = 1.00E-05      
+PVAG     = 0.01           DELTA    = 0.10           NGATE    = 1.0E19        
+MOBMOD   = 1              NQSMOD   = 0              NOIMOD   = 1             
+CAPMOD   = 3              XPART    = 0.5            CGSO     = 9.00E-11      
+CGDO     = 1.50E-11       CGBO     = 0              CGSL     = 0             
+CGDL     = 3.90E-10       CKAPPA   = 1.20           CF       = 0             
+CLC      = 3.0E-09        CLE      = 0.8            DWC      = 0             
+DLC      = 1.90E-07       NOFF     = 3.66           VOFFCV   = -0.40         
+ACDE     = 1.0            MOIN     = 15             CJ       = 2.20E-04      
+MJ       = 0.60           PB       = 0.41           JS       = 1.50E-07      
+NJ       = 1.00           XTI      = 3.0            IJTH     = 0             
+KT1      = -0.45          UTE      = -0.3           PRT      = 5.00E03       
+AT       = 2.5E04         )                                                  
*                                                                             
.ENDL ECH8654                                                                 
                                                                              
*  Device Expression Example                                                  
*    Electrode = Drain Gate Source                                            
*    Mxxx Drain Gin Source Body ECH8654 W=1494310E-6 L=1.0E-6 AD=1494310E-12  
*    RG Gate Gin 15                                                           
*    RB Body Source 0.013                                                     
                                                                              
*  Information herein is for example only;                                    
*  it is not guaranteed for volume production.                                
                                                                              
* ON Semiconductor      
************************* ECH8667 SPICE PARAMETER ****************************
.LIB ECH8667                                                                  
* DATE : 2011/09/15                                                           
* Temp = 27 deg                                                               
* W    =  1494310 E-6 m                                                       
* L    =      1.0 E-6 m                                                       
* AD   =  1494310 E-12 m2                                                     
* RG   =       10 ohm                                                         
* RB   =     0.01 ohm                                                         
                                                                              
.MODEL ECH8667 PMOS (                                LEVEL    = 8             
+VERSION  = 3.2            TNOM     = 27             TOX      = 6.0E-08       
+VTH0     = -1.86          K1       = 3.12           K2       = -0.04         
+NLX      = 1.70E-07       DVT0     = 1.12           DVT1     = 0.38          
+DVT2     = -0.01          U0       = 230            UA       = 8.00E-10      
+UB       = 1.00E-21       VSAT     = 1.25E05        A0       = 0.18          
+AGS      = 0.84           A1       = 0              A2       = 1             
+RDSW     = 8.70E05        PRWG     = -5.0E-03       WR       = 1.22          
+WINT     = 0              LINT     = 8.00E-08       VOFF     = -0.15         
+NFACTOR  = 0.64           CIT      = 0              CDSC     = 2.40E-04      
+CDSCD    = 0              ETA0     = 0.74           DSUB     = 0.96          
+PCLM     = 0.01           PDIBLC1  = 0.00           PDIBLC2  = 1.00E-05      
+DROUT    = 0.96           PSCBE1   = 1.60E09        PSCBE2   = 2.75E-05      
+PVAG     = 0.01           DELTA    = 0.024          NGATE    = 1.0E19        
+MOBMOD   = 1              NQSMOD   = 0              NOIMOD   = 1             
+CAPMOD   = 3              XPART    = 0.5            CGSO     = 1.00E-12      
+CGDO     = 2.15E-11       CGBO     = 0              CGSL     = 0             
+CGDL     = 2.20E-10       CKAPPA   = 2.20           CF       = 0             
+CLC      = 3.0E-09        CLE      = 0.8            DWC      = 0             
+DLC      = -1.00E-12      NOFF     = 0.5            VOFFCV   = -0.01         
+ACDE     = 1.0            MOIN     = 15             CJ       = 1.20E-04      
+MJ       = 0.57           PB       = 0.68           JS       = 5.00E-07      
+NJ       = 1.05           XTI      = 3.0            IJTH     = 0             
+KT1      = -0.5           UTE      = -0.5           PRT      = 8.70E05       
+AT       = 3.3E04         )                                                  
*                                                                             
.ENDL ECH8667                                                                 
                                                                              
*  Device Expression Example                                                  
*    Electrode = Drain Gate Source                                            
*    Mxxx Drain Gin Source Body ECH8667 W=1494310E-6 L=1.0E-6 AD=1494310E-12  
*    RG Gate Gin 10                                                           
*    RB Body Source 0.01                                                      
                                                                              
*  Information herein is for example only;                                    
*  it is not guaranteed for volume production.                                
                                                                              
* ON Semiconductor                                                            

  • Hi Michele,

    You can create you own .subckt using the description provided on that file such as

    .SUBCKT ECH8654TopLevel Drain Gate Source Body

    M1Drain Gin Source Body ECH8654 W=1494310E-6 L=1.0E-6 AD=1494310E-12
    RG Gate Gin 15
    RB Body Source 0.013

    .MODEL ECH8654 PMOS ( LEVEL = 8
    +VERSION = 3.2 TNOM = 27 TOX = 2.7E-08
    +VTH0 = -0.91 K1 = 1.96 K2 = -0.04
    +NLX = 3.20E-07 DVT0 = 1.12 DVT1 = 0.22
    +DVT2 = -0.01 U0 = 300 UA = 1.10E-10
    +UB = 1.00E-21 VSAT = 1.86E04 A0 = 0.44
    +AGS = 1.00 A1 = 0 A2 = 1
    +RDSW = 2.96E03 PRWG = -0.011 WR = 0.83
    +WINT = 0 LINT = 2.09E-09 VOFF = -0.10
    +NFACTOR = 1.118 CIT = 0 CDSC = 2.40E-04
    +CDSCD = 0 ETA0 = 0.08 DSUB = 0.96
    +PCLM = 1.40 PDIBLC1 = 0.05 PDIBLC2 = 6.50E-03
    +DROUT = 0.96 PSCBE1 = 1.40E09 PSCBE2 = 1.00E-05
    +PVAG = 0.01 DELTA = 0.10 NGATE = 1.0E19
    +MOBMOD = 1 NQSMOD = 0 NOIMOD = 1
    +CAPMOD = 3 XPART = 0.5 CGSO = 9.00E-11
    +CGDO = 1.50E-11 CGBO = 0 CGSL = 0
    +CGDL = 3.90E-10 CKAPPA = 1.20 CF = 0
    +CLC = 3.0E-09 CLE = 0.8 DWC = 0
    +DLC = 1.90E-07 NOFF = 3.66 VOFFCV = -0.40
    +ACDE = 1.0 MOIN = 15 CJ = 2.20E-04
    +MJ = 0.60 PB = 0.41 JS = 1.50E-07
    +NJ = 1.00 XTI = 3.0 IJTH = 0
    +KT1 = -0.45 UTE = -0.3 PRT = 5.00E03
    +AT = 2.5E04 )

    .ENDS

    Then you can create symbol for this .SUBKCT as necessary.

    Herman
  • Hi Herman,
    thank you for your answer.
    I will try your suggestion tomorrow.
    Regards,
    Michele
  • Hi Herman,

    I get an error "Not supported MOSFET device model ECH8654 (M1)."

  • Hi Michele,

    Unfortunately, MOSFET Level 8 is not supported by TINA-TI.

    Herman
  • Hi Herman,

    ok thank you.

    Best Regards,

    Michele