Other Parts Discussed in Thread: TINA-TI, LMG1020,
Tool/software: TINA-TI or Spice Models
To whom it may concern -
My questions relate to the evaluation board TIDA-01573 for the FET driver LMG1020.
Referred documents:
- www.ti.com/.../tidrvr3.pdf (Schematic)
- www.ti.com/.../tidrvr4.pdf (BOM)
- www.ti.com/.../lmg (data sheet LMG1020)
1. C10, a bypass cap for the LMG1020, is rated to 85°C. Can you recommend a suitable replacement rated to 125°C?
2. R1, R2, the output resistors at OUTH and OUTL of the XLMG1020 have a value of 0 Ohm (!). Can R1 and R2 be omitted? The data sheet of the LMG1020 states that a single resistor of not less than 2 Ohm can be used instead of R1 and R2 (and OUTH and OUTL be shorted). Is this a viable solution, or is there a stringent reason using two 0 Ohm resistors?
3. What is the function of the shunt resistors R5-R8 parallel to the laser diode? Are they just for board testing if there is no laser? Can R5-R8 be omitted?
I will be very grateful for any information you can provide on these questions.
Best wishes,
Rainer