Part Number: TIDA-00663
Other Parts Discussed in Thread: OPA857
Dear,
I have some questions about the signals coming to the board:
- BP19_PWM_GPIO_TRIGG: I suppose this a pulse.What should be the maximum/minimum length of this pulse?
- TPROP_CALIBRATION_ENABLE_BP10_P3.6: where is this signal used for? Goes it in conjunction with the BP11_CAL signal?
- 5K_GAIN_SETTING_BP9_P3.5: is this used to adapt for different types of diodes?
Thanks for clarifying