Part Number: TIDA-00688
Other Parts Discussed in Thread: LM5017,
We are interested to evaluate this design, it very much matches with our requirement.
Exception is instead of +15,-15V and +5, we need just +24VDC at 40mA
This exception is not that difficult. What I am looking for it is the term Isolation that this design can provide.
What is the isolation between Primary and Secondary in this design?
Additionally, can we get this board for Evaluation?
Our exact requirement is as follows.
Input: 18-36VDC
Output1: 24VDC at 36~40mA at 18VDC Supply
Output2: 24VDC at 36~40mA at 18VDC Supply
For Output 2 I am planning to replicate the whole design on the board, i.e. 2 DC-DCs with 2 nos LM5017 and 2 nos planar.