This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

WEBENCH® Tools: Battery Pack charger design



Tool/software: WEBENCH® Design Tools

I want to design a charger with specs as follows:

Nominal Voltage 72V

Full charge voltage 84V

Output current 10A

for CV & CC mode of operation 

Input is 110VAC-240VAC 10-15A @50hz