This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

WEBENCH® Tools/UCC28600-Q1: Adding svg to schematic form

Part Number: UCC28600-Q1

Tool/software: WEBENCH® Design Tools

Dear All,

how can i upload the svg for power application using the above IC into a schematic??

my power supply requirements are

110-240VAC
48V 5A output

i have the schematic in svg form which open is chrome html , i want to convert it into eagle schematic file and use it for pcb design.

  • Hi Milind,
    You cannot convert the SVG file into a eagle schematic. You can create a WEBENCH design for the inputs conditions using the UCC28600-Q1. Once you are convinced with the design, you will have to draw the schematic in Eagle. We have the export capability (schematic and layout) supported for DC/DC converters but not AC/DC or high voltage DC/DC at the moment.
    Here is a WEBENCH link to the design using UCC28600-Q1.

    webench.ti.com/.../SDP.cgi

    Please let us know if you have more questions.

    Regards,
    Gerold