This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Tool/software: WEBENCH® Design Tools
Dear all,
I have a requirement of a DC DC converter with following specification
Input voltage 18V to 36V
Output1= 3.3V/7.5A
Output2= 1.5V/3A
Input to output isolation required and both outputs(3.3 and 1.5) should be isolated each other.
I am facing problem in giving the isolation requirement. How to specify this isolation requirement in TI Webench power architecture?
Regards
Aneesh
Hi Aneesh,
I could not find a design that exactly meets your specifications, but I found a few that might get you started.
Vin = 18V to 36V, Output Power ~30W
PMP40274 is a synchronous flyback (5V/6A), but with a transformer redesign you could make 2 outputs
PMP4468 is an Active Clamp Forward, this design could also be made to have 2 outputs.
The choice of flyback or forward is really up to the specificiations. The flyback might be lower cost, the ACF will have better efficiency and noise performance.
PMP11107 shows a dual output flyback.
While none of these are exact, hopefully they help get you started.
Thanks,
Robert
Hi Aneesh,
I think you can expect to get 10% regulation on the winding that is not regulated. But this is a function of the transformer design.
Thanks,
Robert
Hi Aneesh,
Again it really depends on the transformer construction. There is no general rule that says one will be better than the others.
Thanks,
Robert