Other Parts Discussed in Thread: MSP430I2020
Tool/software: WEBENCH® Design Tools
Hello,
We are working on Weight scale project with the controller MSP430I2020.
This controller has 24bit Differential input ADC, we use internal Vref 1.2,
Load cell capacity is 300kg,
Load cell output 20mV at 300kg
Please suggest Signal conditioning IC for load cell signal from 0-20mV is converted into 0-1.2V
Thank you