Other Parts Discussed in Thread: BOOSTXL-CC2650MA
Tool/software: Code Composer Studio
I am looking to manufacture a solution for motors using TIDA-01575 Reference Design. I am looking for the most simple solution. Not involving manufacturing processes. I can see that TIDA-01575 calls for 2 kits: MSP-EXP432P401R BOOSTXL-CC2650MA.
But the third element the Signal Conditioning Board is not listed as a product who can be bought at TI Store. So, I assume one can manufacture it using all the data provided in the Design Files. I would like to know if there is a supplier who manufactures this Signal Conditioning Board, with enhancements: for example, the ones mentioned in the same document.
Similarly, the user can change the Kionix KXTC9-3672 sensor with the pin-compatible KX220-1071 or
KX220-1072 to increase the range of vibration up to ±40 g, increase the frequency range of vibration to
9.6 kHz, and easily update the gain and AC response to monitor high vibration machines where low shock
pulses may not require monitoring.
Please help.
Jimmy Saldivias