This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TIDA-050012: Firmware for TIDA-050012

Part Number: TIDA-050012
Other Parts Discussed in Thread: TPS65987D, TPS65981, TPS65987

Hi,

I'd like to use TIDA-050012 to do some USB PD research. Could you please share me with the required bin files. I've got the configuration tools but I can not find any required firmware files in the User guide.

Thanks,

Henry

  • Hi Henry,

    Please download the latest GUI tool and start a new TPS65987D project. It doesn't matter which selections you choose, it just needs to be for the 87D. Next, click on Project --> Import Settings from Project and select the following .PJT file: 5164.TIDA-050012.pjt

    This will ensure you have the latest firmware base image on your board along with the correct settings for TIDA-050012.

    If this answers your question, PLEASE select This resolved my issue

    Thank you,
    Eric

  • Hi Eric,

    Thanks for your reply. The GUI tool I have is called Application Customization Tool downloaded from TPS65987D product page. I can only find 81, 82, 86 and 88DDH in the device list if I start a new project. There is no project device for 87D. Please kindly clarify this for me.  

    Cheers,

    Henry

  • Hi Henry,

    Apologies, but the latest GUI release has an error and did not include 87D templates. Instead, can you select Project --> Load Project and select the .pjt file that I sent in my last post?
    Afterwards, you can select "Change File" under Firmware Base Image and select "TPS65987_88_F707_10_06.bin" which can be found under C:\Program Files\Texas Instruments\TPS65981_2_6_7_8 Application Customization 5.1\tps6598x-application-customization

    Thank you,
    Eric