Hi TI team,
Can you please let me know what is the difference between the thermal design current and maximum current used in the reference design?
As per NXP datasheet of LS2088A the maximum current that the LS2088A can draw from the core voltage rail is 61A. But the reference design has took a maximum current of 120A. So can you please let me know whether I can design for the 61A so that the inductor will be changed to 300nH (PA2607.301NLT- Inductor, Ferrite, 300 nH, 32 A, 0.00031 ohm, SMD) and the same inductor will be used for the core and DDR phases.
Please let me know any specific reason is there behind choosing 120A as maximum current, I hope the design has been done by considering the 60A load transient. Please let me know if any other reason is there.