Part Number: LP3985
Other Parts Discussed in Thread: TINA-TI, , TLV713, MSP430F2101, LP3983, TPS62125, LP2985, MULTIPKGLDOEVM-823, DEM-SOT23LDO
Tool/software: TINA-TI or Spice Models
Hi,
in order to compare startup behavior of LP3985 (2.5V) to TLV713 (2.5V) I am looking for SPICE macros (even encrypted) for both devices to use TINA-TI simulator.
My circuit is powered by a 16.5V battery pack. A buck converter TPS62125 converts 16.5V down to 5V for maximum load current of 100mA. This is also used as the Vin for an LDO, to be chosen between LP3985 or TLV713, to power an MSP430F2101 at 2.5V. Till present I used macros of LP3983 and TLV71310 that seem the only one available similar to LP3985 and TLV71325 but I need to characterize startup time of 2.5V with good reliability in oreder to choose the LDO.
Many thanks
Mauro