Part Number: TIDA-010042
Other Parts Discussed in Thread: UCC39002
Hi All,
Using MSP430F5132 I want to extend following design from TI for
TI Designs: TIDA-010042
MPPT charge controller reference design for 12- and 24-V
solar panels
Requirement:
1) Battery can be charged both from Solar Panel and SMPS (AC to DC) (12V-13.5V, 7A-10A) (maximizing the use of solar panel).
2) Microcontroller or other method should make decision when to do charging from Solar panel or SMPS or both (maximizing the use of solar panel).
3) Load should be supplied from Solar Panel and Battery if power sufficiently available otherwise remaining power to the load should be supplied from SMPS (maximizing the use of solar panel).
3) User is not aware how charging is done or load power is shared but when solar energy is available it should be used (maximizing the use of solar panel).
Please suggest detailed design along with schematic and source code.
Thanks and Regards,
Mithilesh Kumar