Tool/software: WEBENCH® Design Tools
In the setting for the line width, colour, transparency, the 'Transparency' number is actually the line 'density', the inverse of transparency... If I set a transparency of 80%, I expect the line to be mostly transparent, or? But, it works in the opposite sense, where a 'transparency' of 20% gives a density of 20%.
Nit-picking, perhaps, but just trying to get better ;-)