Other Parts Discussed in Thread: TINA-TI
Tool/software: TINA-TI or Spice Models
Hi,
I have read the related BF862 post in the forum but that was back in 2013-14.
The model that NXP has now in their website is somewhat different:
See here: www.nxp.com/.../BF862.prm
* BF862 SPICE MODEL MARCH 2007 NXP SEMICONDUCTORS
* ENVELOPE SOT23
* JBF862: 1, Drain, 2,Gate, 3,Source
.SUBCKT BF862 1 2 3
Ld 1 4 L= 1.1nH
Ls 3 6 L= 1.25nH
Lg 2 5 L= 0.78nH
Rg 5 7 R= 0.535 Ohm
Cds 1 3 C= 0.0001pF
Cgs 2 3 C= 1.05pF
Cgd 1 2 C= 0.201pF
Co 4 6 C= 0.35092pF
Q1 4 7 6 JBF862
.model JBF862 NJF(Beta=47.800E-3 Betatce=-.5 Rd=.8 Rs=7.5000 Lambda=37.300E-3 Vto=-.57093
+ Vtotc=-2.0000E-3 Is=424.60E-12 Isr=2.995p N=1 Nr=2 Xti=3 Alpha=-1.0000E-3
+ Vk=59.97 Cgd=7.4002E-12 M=.6015 Pb=.5 Fc=.5 Cgs=8.2890E-12 Kf=87.5E-18
+ Af=1)
.ENDS BF862
There were a few references as to what modifications must be made to the file contents so that it can be imported into TINA.
I tried the removing the dot before the "SUBCKT" string without luck.
Is there anything else i can do to successfully import that file into TINA in orded to get a valid TSM model file?
Regards
Manos Tsachalidis