This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

WEBENCH® Tools/LMR23615-Q1: Simulation does not have enough phase margin

Part Number: LMR23615-Q1


Tool/software: WEBENCH® Design Tools

Hi Team,

I am trying to use WEBENCH to simulated the LMR23615-Q1 under the following conditions:

Input: 20V - 28V

Vout: 5V

Iout: 500mA

For some reason, the simulation is telling me there is not enough phase margin. Though, I don't think the conditions above are that drastic to be causing instability. Can you please take a look and help me understand why there is not enough phase margin?

Thank you,

Jared