Other Parts Discussed in Thread: TINA-TI,
Tool/software: TINA-TI or Spice Models
From the following link:
http://www.ti.com/product/TPS63030/toolssoftware
How do I utilize these PSPICE files in a TINA-TI simulation? Why are they missing the usual .TSM file? Without the .TSM file, you cannot place a macro in the schematic editor in TINA-TI.
All I want to do is to be able to simulate transient and DC conditions of the TPS63030/1 converters.
I cannot add this file set to the existing TINA-TI libraries because it is missing several files.
Therefore I must ask: what is the purpose of including these file sets, and how can I use them to run a simulation of this converter?