This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TINA/Spice/TINA-TI: TINA/SPICE add temperature behavior

Part Number: TINA-TI

Tool/software: TINA-TI or Spice Models

Hi E2E team,

I am actually trying to simulate a LEDs behavior in function of the temperature :  I am actually testing device between -40C° and 140 C° (  

Run Analysis -> DC Analysis -> DC Transfer Characteristic -> Set Input to “TEMP” & Sweep from -40V to 150V (1V = 1 deg C).

The thing is I'd like to test LEDs forward voltage, and use it in my circuit. But the LEDs that I am currently using are not available in the libraries. I'd like to know if it is possible to create it, or rather take another red LED and add it behavior in temperature through an excel file for example ? As I am looking to simulate mine, i really want to create my own (Vf  vs Temp) curve on an LED.

Any suggestions ?  

Thanks for your help.

Florent