This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

WEBENCH® Tools/TPS51216: TPS51216 D-CAP Frequency

Part Number: TPS51216

Tool/software: WEBENCH® Design Tools

I would like to know about the specifications of TPS51216.
If the output ripple is too small, the D-CAP The jitter may increase and the operating frequency may not be stable.
[reference]
  <www.tij.co.jp/.../jaja465.pdf>

Average: 450 KHz for our on-board power supply with a setting of 400 KHz
It seems that it may move at 2 MHz at the maximum.

[question 1]
In this case, what frequency range should I move?
[Question 2]
I think it has become unstable, but what kind of impact can be considered Is it?
It is understood that the specifications operate with changing frequency, Please let me know.