Other Parts Discussed in Thread: TINA-TI,
Tool/software: TINA-TI or Spice Models
Good day Sir:
So I used the simulation file (SIMPLIS file) that I found on the UCC28780 site, the controller on the simulation is not working when I run a simulation, I used an AC signal source, 60Hz with a bridge rectifier connected and a bulk capacitor, instead of a dc supply. My question is, how come it is not working? I used 127V as peak value on the AC source.
Thanks mate,
-RMV