This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TINA/Spice/TPS62130: Question about AGND and ETPAD connections and effects in the TINA-TI model??

Part Number: TPS62130
Other Parts Discussed in Thread: TINA-TI

Tool/software: TINA-TI or Spice Models

Hi there TI folks;

I'm doing some simulations with a few TI SMPS parts, and I'm interested in their behaviour when connections are bad, or no-connect, or mis-connected.

I tried to run the 62130 model with AGND left 'open', and the simulator failed with some kind of convergence failure... so, I connected the AGND with a 1G Ohm resistor, to simulate a 'bad' AGND, and even isolated the ETPAD pin the same way, but the simulation showed the same behaviour as with AGND connected, and 'probing' those nodes showed a hard GND/0 V on the simulation output.

Thus, the question remains: are these 'pins' actually simulated, or just shown on the schematic for fun??

Best regards,