Part Number: TIDA-00274
Other Parts Discussed in Thread: DRV8313
The Feature list for the TIDA-00274 BLDC motor reference design lists the max current as 1.9Apk/1.25Arms, and the test data shows a test at this limit. However, the reference design uses the DRV8313 EVM hardware which states it can handle 2.5A pk.
What limits the max current in the TIDA-00274 design? Is this a limit set by the control algorithm?