Part Number: PMP21479
Other Parts Discussed in Thread: UCC28780,
If we don't need PD solution, only a simple 65W 19V output adaptor, can it handle 200% peak load for 2mS?
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi Hsu,
We would need to make sure that the transformer core does not saturate as 2ms is a long time. In addition we would need to review the current limit setting. I am looping in the designer for this board. He will advise.
Thanks,
Ryan
Hi Hsu,
The UCC28780 controller allows transient over power conditions up to 115ms, so yes, you can support this application with a design very similar to PMP21479.
The PD controller on the output of PMP21479 will limit the output current to just over 3A, but with a fixed 20V output, you would remove the PD controller. This design has not been tested for these conditions, so I do not know what oher side-effects might happen. Saturation of the core during the peak power event would be one concern.
thanks,
Brian