Part Number: TIDA-01505
Hello,
Had query on Active Startup circuit:
1. STP03D200 BJT has minimum hfe value of 230 and 200 for Ic=20mA and 30mA, why is the assumed hfe value is 500?
2. Rstart_slow value calculated tells it should be <150Mohm, But the value selected is 6 instances of 1.5Mohm which comes to around 9Mohm. Let me know the reason for selecting so low value