This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Dear All:
I design the 20s BMS as the TIDA-01093 , I have 2 question about the TI design. As below shown
1. I think the MCU SDA , CLK signal can through the Q9, Q10 parasitic diode to connect the BQ76930, that can't by the I2C_CTRL_B control. Is it right?
2. in the I2C isolation application with the ISO1541, I think there is only needs one power cut off the communication. Why do you need to control both power sources? I2C_CTRL_B_U& I2C_EN_U?