This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TIDA-01536: TIDA-01536

Part Number: TIDA-01536
Other Parts Discussed in Thread: XTR111

We are having some issues with XTR111 susceptibility to external noise.  For example, when we perform the  IEC61000-4-6: Conducted Immunity test, we are measuring up to 8Vpp noise on a 10V signal.  Based on the reference design testing:
we should be seeing something like 0.2% which is significantly lower than what we are measuring.  To better understand this, can you help us with the following:
- request test details (ie. where and how did they apply the conducted emissions)

- can we get our hands on the reference design board (can't find it anywhere)?