Part Number: PMP11236
Other Parts Discussed in Thread: UCC28881, PMP20745
Hi dear TI Experts,
I want to use PMP11236 reference design for my project. I need to connect one of both 220V AC or 24V DC in the same plug(only one). Thats why I choose this part(It is okay if you suggest another one). And, here is the problem: I want to use it for powering and Arduino board, relay board and 7-segment board. But the PMP11236 says, it is supply 20mA for 5V. Is the PMP11236's power supply okay for this kind of application?
Here is the board that I have designed so far;
Here, I am not using 24V output, only 5V output.
Best regards;
Osman