Other Parts Discussed in Thread: TIDA-010006, LM3480, TIDA-01420, AMC1311, AMC1301, , UCC21530, ISO224, ISO122
Hi,
I am trying to design a 15-20kW AFE motor drive, which consists of an active rectifier and an inverter. I may or may not use the bootstrap DC for the inverter part. But, when the bootstrap is used in the rectifier's gate driver, the modulation index range will be limited. Due to this limited Duty Cycle, for the rectifier part I have to replace it with the Isolated DC/DC converters. I need to use 15/15 DC/DC for the gate driver and 15/5 DC/DC for the ADC current sensing part. Do you have any suggestions from TI products, which is compatible in this application design and works good with the other parts? Also, I need to add three voltage sensors to the rectifier board for the PLL implementation. Do you have any suggestions for that part as well?
Thank you