Because of the holidays, TI E2E™ design support forum responses will be delayed from Dec. 25 through Jan. 2. Thank you for your patience.

This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TIDA-01168: Details on Top Side Interface Material

Part Number: TIDA-01168

Hi Team,

My customer would like to know more details on the interface material between the bus bar and the top side of the PCB on page 10 of TIDA-01168?

More specifically, is the bus bar in direct contact with the copper planes (board top side) or is there an interface material to fill in the air gaps (if any)?

I see that the materials and detailed description are included for the bottom side, but want to understand if it’s the same for the top side.

Thanks,
Mitchell