This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

WEBENCH® Tools: Coil Designer

Tool/software: WEBENCH® Design Tools

Hi everyone,

I designed the following coil with the help of Coil Designer TI WEBENCH

  • Outer Diameter (Dout): 40 mm
  • Number of Layers: 2
  • Turns per layer: 35
  • Trace width (W): 0.2 mm
  • Spacing between Traces (S): 0.2 mm
  • Inner Diameter (Din): 12 mm
  • Space between 1st layer and 2ndlayer(x12) = 1.5 mm

This gave me L=94.8 uH, but after fabrication and measurements, it always gives me 4 uH. 

Any help?

I have pictures for the coil and the measurements if needed.