This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

WEBENCH® Tools/LM5161: Not able to design buck converter in that are in the specs

Part Number: LM5161


Tool/software: WEBENCH® Design Tools

Dear Sir/Madam,

I am trying to design a Buck converter with an input voltage between 4.5V and 85V ( the requirement is from 5-82 but for safety margin I want it to be a little wider).

The lowest voltage that I can use is 5.3V to 85V.

If I look at the specs of LM5161 then it is possible to design a Buck converter with an input voltage range from 4.5V to 100V.

Why is this not possible in the WEBBENCH Design Tools?

It would be very useful for me if it works because I can do simulations with the tool.

Can someone help me or tell me what I missed or do wrong?

I would like to thank you in advance and I am looking forward to your reply.

Regards,

Roberto del Pozo Gallardo