This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Tool/software: TINA-TI or Spice Models
Hello Team,
I'm trying to simulate the output variations to temperature variations(-40 to 85C). My input is a signal 6-17V while my output should be 3.3 V. This works with TPS548A20 with webench model, I attached the result of the simulation. I don't understand
1)why the x axis shows in uC? I inserted as parameters (-40 to 85)
2) the signal generator is set arbitrarly, as a ramp going from 6V to 17V. why the waveform are not shown?
Note That TINA-TI does not tell about any error before performing the simulation.
Hi Elisa,
Please use the attached .TSC file and do the following steps to get output variation to temperature variation.
1. Go to Analysis option and click on DC Analysis
2. Then click on Temperature Analysis and a window like below will open up
3. Here you could insert values for temperature range with no of points
Below is the the results of the output variation to temperature variation
Hope this will help you.
Best Regards,
Ashis
I did not understand how to plot Vout (that's what I need).
Can you include in this webench model (exportable in TINA-TI) also the input signal? (for example a triangle waveform of 11 V with a DC offset of 6V).
I tried to include it in my model but it did not work with the thermal simulation.
Best regards
Elisa
Hi Elisa,
Thanks for your patience.
Unfortunately, thermal characteristics of this device is not modelled. Hence you cannot observe any changes in the model simulation results w.r.t temperature.
Sorry for the inconvenience.
Please let us know if you need any further assistance.
Hi Elisa,
Please use the attached TPS548A20.TSC to see the output variation to temperature variation.
Below is the simulation results of all the probed nodes.
Also you could include input signal of 11 V with a DC offset of 6V by doing the following steps:
1.Select Sources from the window shown below and then select voltage generator from that
2. In that choose triangular wave with required voltage with a DC level as shown in the below window.
Best Regards,
Ashis