This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TIDA-01501: TIDA-01501

Part Number: TIDA-01501

Hi

I want to know the turn spec of trans & coil in TIDA-01501

L1: Common choke 7.5mH(T16)

L2: Common choke 3mH(T16)

L3: PFC coil 400uH(PQ3240)

L4: LLC Inductor 32.8uH(PQ2016)

T1: Trans 230uH(PQ3228)

Thanks