Part Number: TIDA-00961
Dear "Watermelon Noodles",
thank you for your help. There are some more questions appearing:
1) How much bulk capacitance did you use? Which voltage rating? C=? Vmax=?
2) You wrote: "check your power stage can work well with DC input and open loop condition;"
Do you mean to apply a DC voltage in the place of the ac input voltage and to create a boost converter?
In the C-code, I found the definition
// Check system under DC condition (cleanest SFRA curves) 0 is FALSE, 1 is TRUE
#define DC_CHECK 0
Does this mean that if I define this to 1, then I can supply a DC voltage instead of an ac voltage and the controller runs in open loop, boosing up the applied voltage? I will be happy for some more explanation about this "DC_CHECK" variable and how to use it correctly.
3) I already found out that the flyback auxiliary supply starts at about 120V. So increasing the voltage slowly from 0 to 120V, I can do this, but operation I will not see below 120V.
Many thanks.
Best regards
Patrick