Other Parts Discussed in Thread: TINA-TI,
Tool/software: TINA-TI or Spice Models
LM25011 Tina-Ti simulation is giving error.
Plz help to resolve
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi Abhishek,
Could you please attach your test circuit (.TSC file) here?
Thanks & Regards,
Arpan Gupta
Hi Abhishek,
I am able to replicate the issue now and to fix it I have changed the value of Shunt conductance to 1f from 0 in Analysis parameters setting. PFA the updated test bench 4452.CSA-MAIN-1.TSC.
Thanks & Regards,
Arpan Gupta
Hi,
Even i tried to change it but plz see the simulation updated the ip voltage is 12 V unit step but multimeter shows 6.99E-19 V!
Hi Abhishek,
The model you are using is a transient start-up simulation model. Hence, when we simulate for DC OP, simulator shows the node voltages at t=0. As the input source is a step voltage, simulator finds input voltage ~0V at t=0. This is why you are observing very low input voltage (~0V) in DC OP simulation.
As this is a transient start-up simulation model, I would suggest you to do transient simulation. Then you will observe node voltage change with respect to time. I think you are interested in observing steady state node voltages. Hence, if you make a transient simulation, after start-up device will reach steady state. Then you can observe every node voltage at steady state. (To start transient simulation press CTRL+ALT+T and then hit ENTER)
Thanks & Regards,
Arpan Gupta