What changes required in this design if i want to run 60V-250Watt Three Phase BLDC motor on this design?
I want detailed answer which covers all the areas where changes are required.
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
What changes required in this design if i want to run 60V-250Watt Three Phase BLDC motor on this design?
I want detailed answer which covers all the areas where changes are required.
Hello Abhil,
I am going to assign this thread to an expert on the overall board design. My area of concentration is related to the half bridge gate driver IC.
Regards,
Richard Herring
Hi Richard,
Thanks for your attention.
Still i didn't get any reply from design experts.
I want reply as fast as possible.
Thanks,
Abhi
Abhi,
the author of the reference design is out of the office at the moment. I briefly checked the design and I believe that it is compatible with the 60V/250W motor out of the box. No modifications needed. Output mosfets are rated to 100V. The design was tested with Specialty motor rated for 60V (Figure 148 and the picture above).
Best Regards, Jiri Panacek
Hi all,
Thanks.This resolved my issue.
I appreciate support from TI.
Regards,
Abhi