Part Number: TPS61022
Tool/software: WEBENCH® Design Tools
I want to design a DC/DC boost converter and using Webench, I have it narrowed down to two different chips. Parameters are:
Input: DC 3.2V - 4.1V
Output: 5V at .1A - 1.8A
Temp: 50 deg C
I like the TPS61022 design better because it has fewer components and is a bit more efficient. However the Webench design tool won't show the schematic. On the "Select a Design" page it just says "Loading schematic...". And when I click on SIMULATE, it says "Design cannot be created! Your preferred device does not work with the inputs you selected."
Looking at the datasheet, I can't see why this part wouldn't work. Is there a problem with Webench?
Thanks,
Doug