Other Parts Discussed in Thread: TMS320F28035, TDC1000-C2000EVM
Hi, I've developed a Custom board like TIDA-00322, using ATMega328P instead of TMS320F28035. I've checked the board using an oscilloscope and the waveforms that I'm receiving are matching to those mentioned in the datasheet. I'm using Arduino for writing the code. I wish to use TDC1000-C2000EVM GUI for debugging purpose by changing the register values but that's not happening. After connecting my board to the Laptop, and selecting the COM13 as the Serial Port from the Setup tab in the GUI, and clicking connect, "Connect Failed! Check the COM port number." I've tried plugging the device into different USB ports, but the result is the same. Also, COM13 is the only port available, therefore there's no chance of selection of wrong COM port.
Is the connection of GUI to the Custom board running on ATMega328P not possible or what? Help would be much appreciated.
Thanks & Regards