This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

WEBENCH® Tools/LMZ20502: LMZ20502

Part Number: LMZ20502

Tool/software: WEBENCH® Design Tools

Using Webbench my 5V to 3.3Vdc circuit puts out 4.1V. The resistor values suggested Rfbt= 232K in parallel with 12pf and Rfbb= 51.7K

What causes this error? Is there a minimum load for this part? There is 22uF on the output and it is lightly loaded. The mode pin is grounded.