This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

WEBENCH® Tools/LM25117-Q1: To high Duty Cycle allowed in WEBENCH

Part Number: LM25117-Q1


Tool/software: WEBENCH® Design Tools

WEBENCH setup:

LM25117QPMH/NOPB
Switching Frequency: 225.616kHz
Input: 5.3V to 38V
Output: 5.05V@4.5A
Duty Cycle: 97.12% at Vin = 5.3V

According to datasheet the maximum Duty Cycle is 90% at the selected Switching Frequency:

Best regards
Kim