This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TINA/Spice/UCC3895: ucc3895 TINA issue

Part Number: UCC3895
Other Parts Discussed in Thread: TINA-TI,

Tool/software: TINA-TI or Spice Models

Hi team

I installed TINA-TI for simulation, but the problem happened on the ucc3895, the problem is: when I add a 1% PWM pulse in SYNC pin ,the system was stop, and pin CT without signal output , also the OUTA,OUTB....  I want to know whether ucc3879 cannot add the extra clock in SYNC , I had check the datasheet ,the Sync pin is bidirectional interface , that means I can use the external CLK ,use the SYNC as the input pin .

I had test that if I do not connect the external wave , the device performance is OK. When I connect the SYNC , the output will stop.

Can you help me to solve this isssue.

Thank you very much

Leon.Liu