Part Number: TIDA-01505
Other Parts Discussed in Thread: UCC28C43,
Hi,
Below are few queries related to PWM controller, could you please reply on below queries.
- Does UCC28C43 have variable duty cycle linearly or will only function as switch from 100% on to ~0% duty cycle? Mentioned datasheet value of Vfb for PWM duty cycle 2.6<Vfb<2.4 seems to be operating as switch
- There are few instances where set frequency of PWM go to half the ser frequency and 50% duty cycle.
Regards
Smitha M S