Tool/software: WEBENCH® Design Tools
Hi team,
When simulating the LM5175 in Webench the following options are available to probe for a waveform.
Would you have the possibility to add the M1, M2, M3 and M4 gate signals as probe options?
M1: HDRV1
M2: LDRV1
M3: HDRV2
M4: LDRV2
In an ideal case, it would be possible to derive the states of these pins from Vsw1/2 but as deadtime is playing a role, this is not straightforward.
Thanks,
Gustaf