Hi Expert,
I am using the PMP20367 reference design for one of my projects. My questions are:
1. Which heatsink part number is recommended for use with the rectifying diodes(D23,D24,D25 and D26) used in the circuit.
2. Do I need to use insulation to isolate the tab and the heatsink from each other.
3. If insulation is not used should heatsink's mounting terminals be connected to the rectifying diode's cathode through the PCB.
Thank you,
Regards,
Mikha.