Part Number: TIDA-01023
Other Parts Discussed in Thread: LMK04828, ADC12DJ3200, LMX2594
In TIDA-01023,the master LMK04828 SDCLKout1 should be DC-coupled to the slave LMK04828 CLKin0.
I assume that the slave LMK04828 CLKin0 should be used as SYNC input.
The SYNC input should always stay low and accept a positive pulse,so it can not be AC-coupled.
Looking at the default configuration of the LMK04828 EVM,the SDCLKout1 is LVPECL16 and there should be a termination resistor(100 ohm) on the slave LMK04828 CLKin0,but I can not find it.
I also can not find some differential DC-coupling method or specification(like internal bias voltage,input impedance) on the LMK04828 datasheet.
That makes me confused.
Another qusetion is that the ADC12JD3200 SYSREF input should always stay low and accept a positive pulse too,like SYNC input ,but TI recommends AC coupling for SYSREF input .
So I assume that the internal structure will keep SYSREF input low when there is no driver.
Or I should enable SYSREF receiver before SYSREF event and disable SYSREF receiver after SYSREF event.
Thanks.