This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TIDA-00961: availability of datasheet of inductor regarding

Part Number: TIDA-00961


The boost inductors (L102,L103) which u have redesigned is 15uH and the part number is 019890300R . But it is not updated in gerber. Can you please provide the data sheet of the old inductor( nductor, Toroid, Ferrite, 327 µH, 0.065 ohm, TH). The part number is 7840-09-0014.