Part Number: TIDA-00961
Other Parts Discussed in Thread: LP2986
Hi,
Can you please confirm the component U304 used in the circuit is LP2986AIMM-3.3/NOPB. The pitch mentioned in the gerber is 0.65mm which is for the SSOP Package ICs only. But no SSOP packages are available for LP2986 ICs .Only SIOC ,VSSOP and WSON are the available packages. Can we use VSSOP Package LP2986AIMM-3.3/NOPB as U304 for the same footprint.