I build high-end tube guitar amps in one of which, currently I use a combination of three Mean Well power supplies to get 450V @ 500mA, 6.3V at around 2.5A and a 12V in the order of around 250mA. I am looking to move on from that because various aspects are non-ideal.
The PMP20612 schematic looks like it might be flexible enough, but I just do not have the knowledge or expertise to do this.
If someone could kick me in the right direction I'd be delighted.
I am thinking of getting a couple of pcbs fabricated (from the gerbers on the PMP20612 dev page) but need a wiser person than me to explain why that board will not work, if indeed it will not!
Many thanks in advance.
Steve Crow