This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TINA/Spice/TLV2172: About op amp parts data

Part Number: TLV2172
Other Parts Discussed in Thread: TINA-TI, , TLV172

Tool/software: TINA-TI or Spice Models

Hi,

I would like to use TLV2172 in TINA-TI's schematic editor but it is not present in the op-amp drop-down menu.
What should I do?

  • Hi,

    Please find the TINA-TI spice model and ref-design here,

    You can download these and open and simulate the model .TSM in TINA-TI.

  • Hi,

    thank you for your answer.

    TINA-TI is installed in the following folder.

    C:\Program Files (x86)\DesignSoft\Tina 9 - TI

    1. Download the sboma.tsc file in the following folder
         Is it ok?

       C:\Program Files (x86)\DesignSoft\Tina 9 - TI\EXAMPLES\TI Test Circuits

    2.Should I also download sboma93a.zip and put it in a folder below that file?

     (1)TLV172.lib&TLV172.tld

            C:\Program Files (x86)\DesignSoft\Tina 9 - TI\SPICELIB

       (2)TLV172.tsm

           C:\Program Files (x86)\DesignSoft\Tina 9 - TI\MACROLIB

    Is there anything else I need to do?

    Best regards,

  • Hi,

    You don't need to download anything more.

    You can directly copy and use the already placed macro from Ref-Design file in you design file .

    Or you can Go to Insert --> Macro , to choose and insert the .TSM file downloaded(in the zip package).