Part Number: TIDA-00555
Other Parts Discussed in Thread: DCH010505D, SN6501, ISO224, AMC1100
Tool/software: WEBENCH® Design Tools
In TIDA-00555 AMC1100 is used for AC voltage sensing, in which isolated power supply for sensing circuit is designed with SN6501 and transformer then +5V is generated by TLV70450(LDO) and -5V is TPS7A3001. Transfer is difficult to find and have EMI, so i used DCH010505D to produce +5V and -5V for hot side power generation and I will give 3.3V for cold side from microcontroller. my question is that is my schematic fine or have any issue ? and for single ended output do i need 1.65V level shifting ? and could you please suggest me which one has high output BW either AMC1100 or ISO224 and which one is better for AC measuring thanks